View my account

D405 post processing parameters

Comments

1 comment

  • MartyG

    Hi Haris Sivic  Not all of the RealSense Viewer tool's settings, like the ones that you quoted, can be exported to json file.  An example of this is the Histogram Equalization depth visualization setting, which is not a camera hardware feature and so cannot be exported to json.  Instead, Histogram Equalization is applied through the depth colorizer feature that color-shades depth data according to the depth visualization settings.

     

    Post-processing filters are also software-based features that are applied to camera data in real-time and processed on the computer's CPU, not in the camera hardware.

     

    Settings that cannot be defined in a json file can be configured with RealSense SDK program scripting in languages such as C++ and Python.

     

    Further information about this subject can be found at the link below.

    https://support.intelrealsense.com/hc/en-us/community/posts/4441403077395-Realsense-viewer-Ability-to-preset-settings-

    0
    Comment actions Permalink

Please sign in to leave a comment.