error 9986 intel streaming profile is not supported or configuration failed.
I want to calibrate my cameras with CalibrationTool-2.12.0.0. I persistently received this error.
-
Hi Mohammadmahmoodi8020 Please try resetting the calibration of your cameras to their factory-new default calibration in the RealSense Viewer tool with the instructions at the link below.
https://github.com/IntelRealSense/librealsense/issues/10182#issuecomment-1019854487
-
The error message error 9986 intel streaming profile is not supported or configuration failed has not been previously reported.
Instead of using version 2.12.0.0 of the Dynamic Calibration tool, are you able to instead calibrate the camera using the On-Chip Calibration option in the drop-down menu of the More option near the top of the RealSense Viewer's options side-panel?
Also, may I ask whether you have installed the RealSense UWP driver at the link below on your computer? If you have then this driver is not required for using RealSense cameras with Windows and has been known in the past to cause errors with the Dynamic Calibration tool.
-
Although you are using a USB 3 connection, I wonder whether it is being mis-detected as USB 2.1. The Dynamic Calibration tool requires USB 3. If it was attempting to use a resolution of 1280x720 at 30 FPS then that streaming profile would not be supported on your D435 on USB 2 (which only supports 6 FPS at 1280x720 resolution).
You can check whether the camera connection is being detected as USB 3 or USB 2.1 by looking at the number beside the camera name at the top of the RealSense Viewer's options side-panel.
-
Thank you. Next, let's test for the possibility of a corrupted calibration table inside the camera, which can prevent the Dynamic Calibration tool from working when run. The calibration table can be repaired by running a procedure called a gold reset. A gold reset can be performed using the CustomRW program that is installed when the Dynamic Calibration tool is installed, so you should already have it on your computer if you have installed Dynamic Calibration.
Open the Command Prompt text interface on your Windows computer. Then activate the factory reset function of CustomRW by launching the tool in the Command Prompt window with the command below:
Intel.RealSense.CustomRW -g
-
Thank you very much for your patience. Please next try downgrading your camera firmware from 5.14.0.0 to the previous version 5.13.0.50 to test whether there is an incompatibility with 5.14.0.0, which was released after version 2.12.0.0 of Dynamic Calibration was released on 23 August 2022.
https://dev.intelrealsense.com/docs/firmware-releases#d400-series-firmware-downloads
If you have installed the current latest version 2.53.1 of the RealSense SDK using the installer program Intel.RealSense.SDK-WIN10 then I would recommend not downgrading from 5.14.0.0 though.
-
Firmware 5.14.0.0 is the recommended firmware for use with SDK version 2.53.1 and there has been a report of an error when using 5.13.0.50 with 2.53.1. So I would recommend staying with your current 5.14.0.0 firmware if using SDK 2.53.1.
You stated that you are using a high-quality USB 3.0 cable. Is this a long length cable of your own choice? If it is, have you tried using Dynamic Calibration with the official 1 meter USB cable supplied with the camera?
-
Let's try the previous 5.11.0.0 version of the Dynamic Calibration tool. I located a zip file for this version and uploaded it to Google Drive so that you can download the zip from there and extract its contents to run the installer program.
https://drive.google.com/file/d/1c3dDvgsEkLuIkP9SPlYf2WQVDYEvjGi-/view?usp=sharing
The download can be launched by left-clicking on the download icon on the Drive page.
-
At this point we have tried everything that could be attempted to resolve a problem with launching the Dynamic Calibration tool and you have stated that it also occurs on several of your cameras and with different computers. I would therefore recommend going back to On-Chip Calibration. If you create a new issue for that on this support forum then I will be pleased to work with you to improve your calibration results with On-Chip.
Please sign in to leave a comment.
Comments
19 comments