View my account

D457: GMSL to USB or Ethernet

Comments

6 comments

  • MartyG

    Hi Roman Leuzinger  Although the D457 has a USB port, it is intended for use in debugging or production line testing and the camera should be used with a GMSL FAKRA cable.  A 1000 mm / 1 m cable is supplied with the camera.

     

    The D457 is also not a 'plug and play' camera like other RealSense 400 Series camera models are.  Intel can provide a driver for AGX Xavier developer boards to customers who have a non disclosure agreement (NDA) with Intel.  If an AGX Xavier computing board is not being used then the driver must be ported by the customer for use on their particular computing device.

     

    Additionally, a de-serializer component that contains Maxim technology is required to decide the streams.  Intel can supply a de-serializer product if customers contact the RealSense sales team, or alternatively a de-serializer by another provider that contains Maxim technology can be used.

     

    Given your requirement to use a USB connection rather than GMSL FAKRA, the optimal solution may be to use a Chameleon XS commercial enclosure product for RealSense D415, D435 and D455 USB cameras that has IP66 and IP67 protection.

    https://www.autovimation.com/en/enclosures-en/chameleon-xs-realsense-en

    0
    Comment actions Permalink
  • Roman Leuzinger

    I contact the Sales team. I find only the product below. But no specification for it.
    https://store.intelrealsense.com/buy-intel-realsense-des457.html?_ga=2.224848922.1400676547.1675155075-1359367760.1664806747

     

    Is there any chance that the products which I have found by research can work?

    Entron EUSB001/002
    http://www.entroninc.com/prouduct.html

    Other camera vendors do have such bridges but do not sell them standalone:

    Leopardimaging LI-GMSL-USB
    https://www.leopardimaging.com/product/autonomous-camera/maxim-gmsl-cameras/li-ov10635-ser/li-usb30-ov10635-ser-112h/

    e-con 
    https://www.e-consystems.com/gmsl-Kamera-for-nvidia-jetson-tx2-de.asp#ar0330-camera-key-features

    0
    Comment actions Permalink
  • MartyG

    I will refer your question about whether a GMSL to USB convertor device can work with D457 to a team member of this Intel RealSense Help Center forum.  Thanks very much for your patience.

    0
    Comment actions Permalink
  • Rizvi, Sahira

    Hi Roman,

    A GMSL to USB conversion device to allow GMSL connection to be attached to a USB port likely would not work. The D457 already has a USB port that is designed for debugging and not normal camera operation.

     

    0
    Comment actions Permalink
  • Javier

    Can we at least use the USB port for development purposes?

    0
    Comment actions Permalink
  • MartyG

    Hi Roman Leuzinger  I have received information from Intel that it is fine to use the D457 only in USB mode and it has the same USB performance and the same feature-set as the D455, with the added IP65 dust and water protection.  So it is absolutely valid to purchase the D457 for the protection and use it as a USB camera instead of in GMSL / FAKRA mode.

    0
    Comment actions Permalink

Please sign in to leave a comment.