View my account

What's the point in using an external HW trigger or a SW trigger for L515?

Comments

1 comment

  • Jesus Garcia

    Hello Alessio,

    There is no description of the external triggering mechanism on the librealsense SDK Github page but the Multi-Camera Configurations with L515 whitepaper provides a description. Notice in the whitepaper that the use case example is of a static object with multiple cameras around the object capturing frames from different points of view. This is the main use case for multiple L515 cameras. As you correctly pointed out, it is challenging to capture fast-moving objects with this mechanism.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.