Is slam application possible on raspberry pi 4 with t265 camera?
I want to use t265 camera with raspberry pi 4 for indoor drone application. Can I get enough slam performance from pi 4 with the camera t265? Or what are the alternative boards you would recommend.
-
Hi Eremteknoloji,
Since Intel RealSense T265 computes all tracking data on the device, the only hardware requirements are a USB 2 or USB 3 connection that provides 1.5W of power, along with enough memory and compute to boot the T265 and receive the pose data and use it in your application.
Hence, Raspberry Pi 4 is quite enough to have good slam performance.
Regards,
Yu-Chern
Intel RealSense Customer Support
Please sign in to leave a comment.
Comments
2 comments