F455 firmware error
Hello I have a new F455 when I open the Intel RealSense ID viewer I get the following error. Do you have update firmware 2.4 based on the image?
-
Hello Rojiroy,
F450_2.6.0.74_SIGNED.bin can be found in the Assets section of https://github.com/IntelRealSense/RealSenseID/releases/tag/v0.17.1.
If you cannot update the firmware using the RealSense ID Viewer, then use the rsid-fw-update tool. You will have to build the RSID SDK before using the fw update tool.
Sincerely,
Jesus G.
Intel Customer Support -
@...,
I got the following warnings during the update process. How can I do the update?
I also want to update the software on ubuntu 16.04, I would appreciate if you could help.
Output:
./rsid-fw-update --file F450_4.2.0.8200_SKU1_SIGNED.bin --port /dev/ttyACM0
Using manual device selection...[2021-07-29 15:18:12.100] [debug] [LinuxSerial] Opening serial port /dev/ttyACM0 baudrate 115200
[2021-07-29 15:18:12.674] [info] [FwUpdater] Extract modules from "F450_4.2.0.8200_SKU1_SIGNED.bin"
[2021-07-29 15:18:12.674] [debug] [FwUpdater] [ OPFW] 2.76 MB, 6 blocks
[2021-07-29 15:18:12.719] [debug] [FwUpdater] [ NNLED] 2.64 MB, 6 blocks
[2021-07-29 15:18:12.737] [debug] [FwUpdater] [ NNLAS] 2.28 MB, 5 blocks
[2021-07-29 15:18:12.748] [debug] [FwUpdater] [ DNET] 2.95 MB, 6 blocks
[2021-07-29 15:18:12.765] [debug] [FwUpdater] [ YOLO] 1.04 MB, 3 blocks
[2021-07-29 15:18:12.771] [debug] [FwUpdater] [ RECOG] 4.32 MB, 9 blocks
[2021-07-29 15:18:12.796] [debug] [FwUpdater] [ AS2DLR] 2.30 MB, 5 blocks
[2021-07-29 15:18:12.809] [info] [FwUpdater] Extracted 7 modules
[2021-07-29 15:18:12.809] [debug] [FwUpdater]Summary:
* Serial number: 11476228093499A27FM10464-100
* Serial port: /dev/ttyACM0
* Incompatible with current device firmware
* Compatible with new device firmware
* Firmware update path:
* OPFW: 2.8.0.7 -> 4.2.0.8200
* RECOG: 20.12.20.0 -> 1.6.21.0[2021-07-29 15:18:12.810] [debug] [LinuxSerial] Opening serial port /dev/ttyACM0 baudrate 115200
[2021-07-29 15:18:13.259] [info] [FwUpdater] Extract modules from "F450_4.2.0.8200_SKU1_SIGNED.bin"
[2021-07-29 15:18:13.259] [debug] [FwUpdater] [ OPFW] 2.76 MB, 6 blocks
[2021-07-29 15:18:13.300] [debug] [FwUpdater] [ NNLED] 2.64 MB, 6 blocks
[2021-07-29 15:18:13.316] [debug] [FwUpdater] [ NNLAS] 2.28 MB, 5 blocks
[2021-07-29 15:18:13.328] [debug] [FwUpdater] [ DNET] 2.95 MB, 6 blocks
[2021-07-29 15:18:13.344] [debug] [FwUpdater] [ YOLO] 1.04 MB, 3 blocks
[2021-07-29 15:18:13.349] [debug] [FwUpdater] [ RECOG] 4.32 MB, 9 blocks
[2021-07-29 15:18:13.371] [debug] [FwUpdater] [ AS2DLR] 2.30 MB, 5 blocks
[2021-07-29 15:18:13.384] [info] [FwUpdater] Extracted 7 modules
[2021-07-29 15:18:13.384] [debug] [FwUpdater]
Firmware cannot be updated directly to the chosen version.
Flash firmware version 3.1.#.# first.
Please sign in to leave a comment.
Comments
2 comments