Maximum Range(Distance) that "Short-range" Preset can give depth with XGA resolution.
What is the Maximum distance that short range preset can cover with XGA (1024x768) Resolution in L515?
-
Hi Aravindjag,
Based on the L515 datasheet (page 8, Table 3.1 Depth Camera Specification), the maximum distance for L515 with XGA Resolution (1024x768) can reach up to 2.6m at 15% reflectivity and 6.5m at 95% reflectivity.
Regards,
Yu-Chern
Intel RealSense Customer Support -
Hi Aravindjag,
I've validated that the maximum distance for L515 in "Short Range" Preset Control can reach up to 6.5m which is the same as the L515 datasheet (page 8, Table 3.1 Depth Camera Specification).
Regards,
Yu-Chern
Intel RealSense Customer Support
Please sign in to leave a comment.
Comments
5 comments