View my account

Configure L515 camera without Windows computer

Comments

7 comments

  • Zulkifli Halim

    Hello Katharina,

    Thank you for contacting us.

    The tools you mentioned are all included in the Librealsense SDK and the Linux Distribution can be installed here. Included in the SDK is a file that exposes all the options you can change: rs_options.h (this is part of the Python wrapper). 

    Here is a document that may be useful to you about optimizing the range on your L515. You can also refer to the L515 User Guide for more information. Please let us know if you need any further information.

    Regards,
    Zulkifli Halim
    Intel Customer Support 

    0
    Comment actions Permalink
  • Katharina

    Thanks for the answer! The link to the rs_options.h file is really helpful. I also managed to build the intel realsense viewer for OSx and was able to test some of the configurations.

    Are those configurations saved on the camera once I've set them in the intel realsense viewer? Or are they only a "soft configuration" done by the software itself?

    If it is only a temporary change in the configuration - what is the preset like? Is the camera set to "short range" by default?

    Thanks!

    0
    Comment actions Permalink
  • Zulkifli Halim

    Hello Katharina,

     

    The configuration will back to default. The preset is set as "Default" when you launch the Realsense Viewer. 

     

    Regards,

    Zulkifli Halim

    Intel Customer Support 

     

    0
    Comment actions Permalink
  • Katharina

    I can't see "Default" as an option anymore when I launch the Intel Realsense Viewer. The only options I have are:

    • Custom
    • No Ambient Light
    • Low Ambient Light
    • Max Range
    • Short Range

    Is "Default" similar to any of the other presets? How can I restore the "Default" setting?

    0
    Comment actions Permalink
  • Zulkifli Halim

    Hello Katharina,

     

    When you launch the RealSense Viewer, the preset will automatically set to default (see attachment).

    I suggest you look at the use full tips In L515 User Guide on page 18.

     

    Regards,

    Zulkifli

    Intel Customer Support

    0
    Comment actions Permalink
  • Katharina

    Hi Zulkifli,

    When I launch the RealSense Viewer, the preset does not automatically set to default. It automatically sets to "Max Range" and when I look at all the options in the drop-down menu, "Default" is not an option anymore. I attached screenshots of both.

    Thanks,
    Katharina

    0
    Comment actions Permalink
  • Zulkifli Halim

    Hello Katharina,

     

    The latest version of librealsense The L500 Default preset has been deprecated. l500-options.cpp line 522 ""RS2_L500_VISUAL_PRESET_DEFAULT was deprecated!" );"

     

    Sincerely,

    Zulkifli

    Intel Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.