View my account

I cannot see my device on the Intel Realsense Viewer.

Comments

21 comments

  • Official comment
    Rizvi, Sahira

    Hi A Samed Cftci I have sent you an email with more information on how to exchange your camera. Please let me know if you have further questions or if you did not receive any communication. 

    Sincerely,

    Sahira 

    Comment actions Permalink
  • MartyG

    Hi A Samed Cftci  There is a simple solution for the non-detection of D457.  By default this camera model is set as a MIPI camera instead of a USB camera and is used with a high-speed GMSL / FAKRA connection like those used in the automotive industry.  D457 can be set to operate in USB mode though, and in this mode it is detected as a D455 with the same performance and feature-set as D455 but with the added IP65 dust and water protection.

     

    To set the D457 in USB mode so that the RealSense Viewer can detect it, please remove a small cap on the top of the camera's casing by inserting a pin in the cap's small hole.  Underneath is a set of hardware sync pins, and also on the D457 model a mode switch.  This switch is set to a position labelled MIPI by default, and there is also a USB position. 

     

    If you insert a pin into the opened recess beside the MIPI position and gently move the pin left towards the 'USB' position until you feel a physical sideward movement, the camera should now be detectable on USB.

     

    0
    Comment actions Permalink
  • A Samed Cftci

    I have already attempted to resolve the issue. Two days ago, my friends, who were using Windows machines, were able to view data from the camera. However, after uploading older firmware to the camera today, I am unable to revert it back to the previous version. Furthermore, my friends are also unable to view data from the camera, resulting in a loss of connection.

    0
    Comment actions Permalink
  • MartyG

    Firmware driver 5.14.0.0 and RealSense SDK 2.53.1 is recommended to be used with D457.

     

    You should be able to upgrade to 5.14.0.0 in the RealSense Viewer. 

    1.  Download the Viewer bin file for 5.14.0.0 to your computer from the link below.

    https://dev.intelrealsense.com/docs/firmware-releases#d400-series-firmware-downloads

    2.  Go to the More option near the top of the Viewer's options side-panel and select Update Firmware from its drop-down menu.

    3.  A file navigation box will pop up.  Navigate to the location on your computer where you downloaded the .bin file to and select the file.  The firmware update should now automatically begin.

    0
    Comment actions Permalink
  • A Samed Cftci

    As you can see, when I connect the camera to my computer, I am unable to see the device on the current version of Viewer(2.53.1), but it appears under USB in the Device Manager.

    0
    Comment actions Permalink
  • MartyG

    If the camera has had its mode switch moved over the USB position then a pair of D455 Depth and RGB drivers should appear in the Cameras section of the Device Manager.  Your one does not have the Cameras icon, suggesting that the camera is not being properly detected.

     

     

    If you are certain that the mode switch in the recess has been moved to the USB position, then please next use the instructions at the link below to check whether the Windows camera privacy settings for accessing the camera are both set to On.

    https://github.com/IntelRealSense/librealsense/issues/3381#issuecomment-503424789

    0
    Comment actions Permalink
  • A Samed Cftci

    Yes, I have followed the steps you provided, but the issue still persists. Since I installed the old software, Viewer is unable to detect my camera. Do I have the option to physically reset or restore my camera to factory settings?

    0
    Comment actions Permalink
  • MartyG

    The RealSense Viewer has a procedure for resetting the camera to factory-new defaults but it relies on the camera being detected, so would not be helpful in this case.

    https://github.com/IntelRealSense/librealsense/issues/10182#issuecomment-1019854487

     

    It may be possible to recover the camera using the firmware update tool rs-fw-update which has a recovery mode.  You can run this tool in the Windows Command Prompt text interface.

    1.  Download the 5.14.0.0 bin file to the location below on your computer.

    C:\Program Files (x86)\Intel RealSense SDK 2.0\tools

    2. Open the Command Prompt and paste the command below into the window with Ctrl_V.

    cd C:\Program Files (x86)\Intel RealSense SDK 2.0\tools

    3.  Input the command below into the Command Prompt window to launch the rs-fw-update tool in recovery mode and use the 5.14.0.0 bin file for the recovery.

    rs-fw-update -r -f  Signed_Image_UVC_5_14_0_0.bin

    0
    Comment actions Permalink
  • A Samed Cftci

    I have also done that, but I encountered an error message stating 'No recovery devices were found!'.(The camera is currently plugged into my computer.)

    0
    Comment actions Permalink
  • MartyG

    Do you remember which firmware version you installed before the camera stopped being detected?

    0
    Comment actions Permalink
  • A Samed Cftci

    Firmware version I installed before the camera stopped being detected is 5_12_13_50

    0
    Comment actions Permalink
  • MartyG

    Firmware 5.12.13.50 would not be compatible with D457 in MIPI mode as it requires a minimum of firmware 5.14.0.0.

     

    5.12.13.50 should be compatible with D455 though, and D457 is identified as D455 when the mode switch is in the 'USB' position.

     

    I would next recommend using a pin to move the mode switch to the 'MIPI' position and then back to the 'USB' position, just to make sure that the switch is fully in the 'USB' position.

     

    Please also try using the link below to download the 2.45.0 version of the RealSense Viewer tool from the 'Assets' file list to see whether it can detect the camera as D455, as firmware 5.12.13.50 was the recommended firmware version for 2.45.0.

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.45.0

     

    0
    Comment actions Permalink
  • A Samed Cftci

    I switched to the 'MIPI' position and then back to the 'USB' position. I am sure that the camera is on the USB mode. Afterwards, I installed version 2.45.0 of Realsense Viewer and it still doesn't detect my device.

     
    0
    Comment actions Permalink
  • MartyG

    I will refer your case to a senior staff member of this Intel RealSense Help Center support forum for further assistance.  Thanks very much for your patience!

    0
    Comment actions Permalink
  • A Samed Cftci

    Thank you. When will you be in touch? The deadline for my project is approaching, and it is of utmost importance that I am able to operate the camera.

    0
    Comment actions Permalink
  • MartyG

    I will emphasize to the Intel RealSense Help Center team member the urgency of your situation.  They are responsive, though I am not a member of the Help Center team (I volunteer assistance here) and so cannot give a time estimate for a reply.

    1
    Comment actions Permalink
  • MartyG

    Can you try unplugging the micro-sized end of the USB cable from the camera, turning the connector around the opposite way and plugging it back in to see whether the camera is now detected, please?  In USB mode the D457 may work only when the connector is inserted in one of the two available insertion directions.

    0
    Comment actions Permalink
  • A Samed Cftci

    I did that too but the camera still won't detect

    0
    Comment actions Permalink
  • MartyG

    In this situation the only remaining option is to return the camera unfortunately, which I understand will be problematic in regard to your approaching deadline.  An Intel RealSense Help Center team member sent you a message about this yesterday.

    https://support.intelrealsense.com/hc/en-us/community/posts/15226169805971/comments/15344671113363

    0
    Comment actions Permalink
  • A Samed Cftci

    Can I solve this problem by disconnecting the FPC module in D4 board with the camera module? Another user who had a fairly similar problem to this had found such a solution. I saw it from the community post on the site.

    0
    Comment actions Permalink
  • MartyG

    A member of the Intel RealSense team that I spoke to who has knowledge on this subject said that the D457 may be recoverable if the ASIC (i.e the Vision Processor D4) is removed. 

     

    Opening the camera up though will instantly invalidate the warranty, though some RealSense users do prefer performing their own maintenance with knowledge of this warning if they have a time-critical situation and the skills to do a repair.  

    0
    Comment actions Permalink

Please sign in to leave a comment.