My Intel RealSense Viewer opens and reports an error and cannot recognize the camera
As shown in the figure, the following error occurs when I open the software
21:58:04 [Error] C:\jenkins_ sys_ rsbuild\workspace\LRS_ windows_ compile_ pipeline\src\sensor.cpp:664 - acquire_ Power failed: MFCreateDeviceSource (_device_attrs,&_source) returned: HResult 0x80070005: "Access denied."
21:58:04 [Warn] C:\jenkins_ sys_ rsbuild\workspace\LRS_ windows_ compile_ pipeline\src\sensor.cpp:1285 - Failed to add Backlight Compensation control for RGB Camera
"I initially thought it was a system problem because my system was Windows 11, but after I tried to run on another Windows 11 and succeeded, I thought it should be a problem with my computer, which was configured as 12500H+RTX2050."
-
Hello, please try using the instructions at the link below to check whether the Windows camera privacy settings for accessing the camera are both set to On.
https://github.com/IntelRealSense/librealsense/issues/3381#issuecomment-503424789
Please sign in to leave a comment.
Comments
1 comment