Need to download dmft_version_6.1.160.21
Hello,
I'm looking download UWP 6.1.160.21.
Support page shows I should be using my setup with firmware 5.12.7.100 and the SDK 2.38.1
When I go to the hyperlink it takes me to only the latest available, .22.
I was hoping to download it through Intel and not anything 3rd party.
https://dev.intelrealsense.com/docs/recommended-production-camera-configurations
Matt
-
Hi Matt Leeper Although the RealSense UWP driver is listed on the Recommended Production Configuration table, it is not required to use RealSense cameras with Windows. Its purpose is to provide an interface with software and hardware that supports Microsoft's Universal Windows Platform (UWP) interface, such as the Microsoft HoloLens headset. If you do not need to interface with UWP-supporting products then the UWP driver does not need to be installed.
If you do need to interface with UWP, only the latest version of the driver is available. Support for the RealSense UWP driver has now ceased.
Please sign in to leave a comment.
Comments
1 comment