de1 arm cortex processor compatibility with the RealSense d435
are there compatible drivers available for the RealSense camera that are compatible with the Arm Cortex processor running on the DE1-SoC board
-
Hi Moumouni Abdoul RealSense 400 Series cameras are compatible with any Arm or Intel processor.
I note that the DE1-SoC product is built around the Altera System-on-Chip (SoC) FPGA. Resources about using RealSense cameras with FPGA boards are listed at the link below.
https://support.intelrealsense.com/hc/en-us/community/posts/6673895808915/comments/6674992093459
Please sign in to leave a comment.
Comments
1 comment