Able to buy 90 degree USB adapter in D455 separately?
I had a pull on the USB cable because the robot arm limits weren't set up quite right in ROS for the amount of cable slack they had. It tweaked the USB connector. We took the back cover off and verified that the camera is still in great shape if we connect up to the USB-C connector internally, but can't seem to find a place to buy that 90 degree PCB connector.
We had been looking for a for-part-only D455 model on eBay, but that hasn't shown up. Is there a way we can purchase just that part from Intel?
-
Hi John Swensen The L-shape adaptor part is not available for separate purchase, unfortunately. I researched possible alternative adaptor parts but most would not fit in the space of the original. A compromise may be to obtain a cable with a 90 degree connector and have the cable hanging out of the bottom of the D455's casing. If you go to Google Images and search for the term 'usb 90 degree cable usb-c' then you can see examples of what I mean.
Please sign in to leave a comment.
Comments
1 comment