Intel T625 dropped during use
“Frames didn’t arrive within 5000”
-
Dear customer,
Thanks for reaching out to us.
May I know which version of Intel® RealSense™ are you using on your machines?
Meanwhile, could you please try the following suggestion and see if your issue was able to resolve?-
Use the latest firmware and RealSense SDK 2.0 version.
-
Connect the camera directly to a USB 3 port on your PC.
If the camera is already connected directly to the PC, try using a powered USB hub.
-
Use the USB cable that came with the RealSense camera.
The cable that came with your RealSense Camera is a high-quality USB cable that is capable of handling the power and bandwidth requirements of the camera. Using other cables is not recommended.
-
Connect the RealSense camera to a different computer - preferably a computer with an Intel processor.
If your camera works on another computer, then the original computer probably has a USB subsystem that the camera is having problems with.
-
Flip the USB C connector that is inserted into the camera and re-insert it the opposite way.
Sometimes the camera will work only if the cable is inserted in a particular orientation.
-
Update the USB drivers on the PC.
You probably already have the latest USB drivers due to automatic Windows Updates but this is worth checking.
Regards,
Wan
Intel Customer Support -
Use the latest firmware and RealSense SDK 2.0 version.
Please sign in to leave a comment.
Comments
4 comments