[ERROR] Could not create device - xioctl(VIDIOC_S_EXT_CTRLS) failed. Last Error: Invalid argument
Hi!
I'm working with a SBC Debix Model A (2GB RAM) and a Debix-Customized Ubuntu 22.04 Image installed on it, also with ROS2 Humble.
I installed "succesfully" (no errors appeared) both Intel SDK and ROS2 Wrapper and I can use all the commands such as rs-enumerate-devices.
I've got a D455 camera correctly plugged as you can see:
debix@DEBIX26:~$ lsusb | grep "Intel"
Bus 002 Device 005: ID 8086:0b5c Intel Corp. Intel(R) RealSense(TM) Depth Camera 455
But when I execute rs-enumerate-devices:
debix@DEBIX26:~$ rs-enumerate-devices
25/07 09:26:26,587 ERROR [281473799996512] (librealsense-exception.h:52) xioctl(VIDIOC_S_EXT_CTRLS) failed Last Error: Invalid argument
Could not create device - xioctl(VIDIOC_S_EXT_CTRLS) failed Last Error: Invalid argument . Check SDK logs for details
Segmentation fault (core dumped)
This error appears. It also appears when executing ros2 realsense2_camera_node I don't know what to do.
-
Hi Jesus Dovale,
Our GitHub collaborator has provided suggestion in the following discussion.
Regards,
Yu Chern
Please sign in to leave a comment.
Comments
1 comment