What are the differences between the D455 vs D456?
Hello,
I was wondering if I could get a thorough explanation of the differences between the Realsense D455 and D456, if any. I see that the difference is the IP65 enclosure rating from the realsense comparison table but was wondering if there is any more differences between the models?: https://www.intelrealsense.com/compare-depth-cameras/
Thanks!
-
Hi Hassanshafi The IP65 casing that protects against entry from dust and water spray is the only difference between the D455 and D456 models.
Please sign in to leave a comment.
Comments
1 comment