depth camera module is suitable up to what moving speed ?
as if i want to put this camera module on some robotic system for what moving speed camera module output will be efficient
-
Hi Raxita Chavda If you will be capturing both depth and RGB then the D450 module should meet your needs, as it has fast global shutters on both the RGB and depth sensors that are suited to capturing high-speed motion, up to a vehicle travelling at high speed on a road.
https://www.youtube.com/watch?v=OwJmCyAn3JQ
If you will only be capturing depth then the D430 module may also be suitable and can also capture at vehicle speed, though it has a smaller field of view size than the D450 module.
If you are able to wait until November 2024 and do not need to depth sense further than a few meters then the new D421 module just announced may be of interest, as it integrates the depth module and the Vision Processor D4 on a single board instead of needing two separate boards.
.https://github.com/IntelRealSense/librealsense/issues/13371
Please sign in to leave a comment.
Comments
1 comment