View my account

Comments

44 comments

  • MartyG

    Is it detected please if you insert it into the USB port with a quick, firm motion instead of inserting it slowly, please?

    0
    Comment actions Permalink
  • Huzaifa Shahid Minhas

    No not at all.

    I'm using high quality cable plumed to usb 3.0 port of laptop

     

    0
    Comment actions Permalink
  • MartyG

    Do you have the original short cable supplied with the camera to test whether the camera is detected with the official cable?

    0
    Comment actions Permalink
  • Huzaifa Shahid Minhas

    Yup I'm using original cable from the box

     

    0
    Comment actions Permalink
  • MartyG

    Do you have another USB port you can try the camera in, please?  The camera should even work in a USB 2.0 port if you have one.

    0
    Comment actions Permalink
  • Huzaifa Shahid Minhas

    I have tried all ports of my laptop and also tried camera on another laptop but in both cases even windows is unable to recognize the camera.

     

    0
    Comment actions Permalink
  • MartyG

    If it is not working on another laptop, it suggests that the problem may be related to the camera's firmware driver.  This driver is stored inside the camera, and so any problems with it will also be carried over to other PCs that the camera is plugged into.

    Can you check also please that the end of the USB cable that goes into the side of the camera is pushed firmly in all the way?   The camera may not be detected if that end of the cable is only partly inserted into the side of the camera.

    0
    Comment actions Permalink
  • Huzaifa Shahid Minhas

    I have also checked it multiple times. Main problem that i'm facing right now is that it is not detected by any port of laptop. Issue regarding firmware can only be resolved once I have any sort of detection of camera by laptop.

     

    0
    Comment actions Permalink
  • MartyG

    Can you check please that permission to access to the camera hardware is set to On in the Windows privacy settings?

    You can find the Privacy window by typing 'privacy' into the search box at the bottom of your Windows screen, next to the button where you shut down the PC. Once the Privacy window is open, select the 'Camera' option in the side-panel.

    Both the 'Allow access to the camera on this device' and the 'Allow apps to access your camera' options should be set to On.

    0
    Comment actions Permalink
  • Huzaifa Shahid Minhas

    Both options are already set to on.

     

    0
    Comment actions Permalink
  • MartyG

    Has the camera ever worked, or has it always been undetectable?

    0
    Comment actions Permalink
  • Huzaifa Shahid Minhas

    It did.

    0
    Comment actions Permalink
  • MartyG

    Going back to the possibility that there is a corrupted firmware driver in the camera, could you check please if the RealSense Viewer program can detect the camera under the name 'RealSense D4xx Recovery'.  If it can, go to the More icon at the top of the options side panel and select the menu option to update to recommended firmware.

    0
    Comment actions Permalink
  • Huzaifa Shahid Minhas

    No, only the platform camera from the laptop is being detected.

    Is there any possibility that the port of the camera is damaged and data signals are not received by the laptop?

    0
    Comment actions Permalink
  • MartyG

    The remaining possibilities include a USB cable gone bad (something difficult to test for it you do not have another USB-C type cable) or a hardware failure inside the camera.  

    It is a very long shot, but you could try putting the camera end of the USB cable into the side of the camera upside down.  USB-C cables are reversible on their micro-size end, so they can be inserted both ways up.  

    0
    Comment actions Permalink
  • Huzaifa Shahid Minhas

    I have tried all of these methods but none seem to be working. I think it is some malfunction in the inside

    0
    Comment actions Permalink
  • MartyG

    If you purchased the camera within the past 30 days then you have the right to return it for a refund or replacement.  If you bought it from Intel's online store then the return claim is filed with Intel.  If you purchased it anywhere else then it should be returned to the retailer that you bought it from.

    0
    Comment actions Permalink
  • Huzaifa Shahid Minhas

    Can you help me to check if there exist any hardware issues.

     

    0
    Comment actions Permalink
  • MartyG

    If the camera is not being detected then there is no way to get information on the state of its components.  If it were detectable, the sensor-control sample program could list which sensors are detected (and so indicate which were not present).

    You could try running the Windows Troubleshoot tool though, which may detect and auto-fix problems.  This link explains how:

    https://forums.intel.com/s/question/0D70P000006JugoSAC 

    0
    Comment actions Permalink
  • Sheethal Ng

    Hi,

    I am facing the same issue. i thought it is related to corrupted firmware.

    But it is working in other laptop (Windows 7 64 bit).

     

    Initially it worked in my Windows 8.1, but in Depth Quality Tool for Intel RealSense Cameras i selected firmware update option, right after that camera is not detected in Windows 8.1.

     

    There is also a issue in HID Sensor Collection driver.

     

    Please let me know what exactly is the probelm

     

    Thanks in advance  

     

    0
    Comment actions Permalink
  • MartyG

    Sheethal Ng   Do you have a D435i, please?  Your mention of the HID Sensor Collection makes me think this.

    0
    Comment actions Permalink
  • Sheethal Ng

    Yes

    0
    Comment actions Permalink
  • Sheethal Ng

    When the camera was working on my Windows 8.1, the Viewer was crashing as soon as i opened it.

    So i tried the other tool Depth control, and updated the firmware.

     

    Right after that the camera is not detected.

     

     

    0
    Comment actions Permalink
  • MartyG

    The D435i is not officially supported on every computer / computing device that the D435 is.  The following is quoted from the RealSense SDK's Releases page:

    "D435i is supported on Linux, Windows 10 and Android. Mac OS support is scheduled next, and Windows 7 will be provided in future releases".  So technically it should not have been able to work on Windows 7.

    If you used the Firmware Update option (the manual installation one where you provide a firmware file) then the firmware version needs to be 5.11.6.250 or newer.  This is because the D435i was launched about a year after the D435, which does not contain an IMU.  So cameras with firmwares earlier than 5.11.6.250 would not have D435i support in them.

    0
    Comment actions Permalink
  • Sheethal Ng

    What solution do u suggest??

     

    0
    Comment actions Permalink
  • MartyG

    If the camera could be detected by the Viewer or by the Depth Quality Tool then you could use the Install Recommended Firmware option in the same menu as Update Firmware. This would automatically install the newest firmware (currently 5.12.5) without having to provide a firmware file.

    If the camera is not detected by either of these programs then you could try the rs-fw-update firmware updater software, which has a Recovery mode for cameras.

    https://dev.intelrealsense.com/docs/firmware-update-tool 

    0
    Comment actions Permalink
  • Sheethal Ng

    I downloaded the firmware and used the following command.

     

    rs-fw-update.exe -f Signed_Image_UVC_5_12_5_0.bin.

     

    But i did not get any output in the cmd

     

    0
    Comment actions Permalink
  • MartyG

    Try it with the -r recovery flag inserted please:

    rs-fw-update.exe -r -f Signed_Image_UVC_5_12_5_0.bin

     

    BTW, is the firmware .bin file placed in the same folder as the rs-fw-update program?

    0
    Comment actions Permalink
  • Sheethal Ng

    yes the .bin file is present in the same folder.

    The output showed

    update to FW: Signed_Image_UVC_5_11_6_250.bin
    0
    Comment actions Permalink
  • MartyG

    Interesting.  Does the camera work now if tried in the Viewer or Depth Quality Tool?

    0
    Comment actions Permalink

Please sign in to leave a comment.