T265 vs T261 specifications
Hello,
Where can we access detailed specs about T265 and T261 modules?
I am rather interested in if the T261 is functionally equivalent to T265 with the exception of casing?
Usually OEM sensors from realsense has one or few features missing compared to the non-OEM sensors, that is why I am asking.
Best regards,
C.A.
-
The data sheet document for T261 and T265 can be found in the link below.
https://dev.intelrealsense.com/docs/tracking-camera-t265-datasheet
The small difference between T261 and T265 is that the T265 adds an 'interposer card' to allow USB connection. The data sheet says this:
"The T265 and T261 have one main board which includes all components on a single board. T265 comprises a T261 module, an interposer card with a USB connector and a peripheral envelope. The T261 module requires an external interposer card to allow USB connection, in case it is used outside the T265 peripheral".
Please sign in to leave a comment.
Comments
1 comment