T261 module
Hi, I want to use the T261 cameras to shoot an image. Is that possible? Can I access the images from the two cameras?
-
You can access the fisheye cameras if you use the device with a USB 3 connection. If it is used in a USB 2 port then only pose data is available, not the fisheye data.
The RealSense SDK software has an example program for showing a fisheye image in a window.
https://github.com/IntelRealSense/librealsense/tree/master/examples/ar-basic
The T261 module requires an external interposer card to allow USB connection.
-
Intel's data sheet document for the T261 module says on page 12 that its fisheye sensor's signal interface has "MIPI CSI-2, 2 X Lanes". Pages 13 to 15 list connector details.
Please sign in to leave a comment.
Comments
3 comments