D455 + T265 3d print mount?
Hi All,
Just got the new D455 realsense camera.
I have been using the D435 in conjunction with the t265 using the 3d printed mount for both cameras from the CAD file that was provided a while ago.
Is there any CAD file available for using the D455 together with the t265?
Seems key to get the two cameras lined up correctly so that the coordinate systems are aligned.
Thanks!
-
I noticed the USB port on the D455 is on the bottom. That may lend itself to quite a different mount than the D435, which has the mount on the side. I might see if i can cad up something in Autodesk. These things are pretty simple to make. The only real question is where the coordinate systems and mounting holes are located on the cameras.
Please sign in to leave a comment.
Comments
2 comments