L515 - Connectivity
Does the box come with a USB C cable?
Can use a USB C to RJ45 adapter to convert the camera to a network device?
-
Official comment
Hi Bettychanlh,
Yes, the box comes with a USB C cable.The camera cannot be converted to a network device by using the USB C to RJ45 adapter. These adapters are used on laptops and tablets where they use the USB C port as a network interface. The laptops and tablets have a network stack installed that allows them to do this. RealSense cameras do not have built-in networking capability.
The only product on the market that has added network connectivity to a RealSense camera is the Framos D435e.
There is no network-enabled, L515-based product on the market.Regards,
Aznie
Intel Customer SupportComment actions
Please sign in to leave a comment.
Comments
1 comment