Realsense L515 prevent interference without hardware sync
Hello!
I am working on a project requiring two Realsense L515 cameras pointed in the same direction. Unfortunately for this project, using hardware sync is not a possibility, as there would be other issues.
I have a period of about 1 second between taking pictures with each of the cameras. I tried turning the cameras on and off again sequentially, but this takes a bit too long (it takes about two seconds to turn it on and get an image, which is not in the time limits).
Is there a way this can be achieved without hardware sync, considering there is a bit of time before each camera has to take a photo?
Thanks!
-
Hi James,
Hardware sync is the only option to ensure the IR from the cameras do not interfere with each other.
Furthermore, I think using the hardware sync should be able to achieve your desired response time as shown in this L515 multicamera trigger timing calculation section.
Regards,
Rizal
Please sign in to leave a comment.
Comments
1 comment