How is the Realsense D435 a class 1 laser product
Looking into the documentation there is defined that the Realsense D435 is a class 1 laser device.
But when looking further into the specifications there is told that the device can also emit a maximum of 360mW.
When looking into the laser class specifications that would make it fall in the Class 3B,
https://www.lasersafetyfacts.com/laserclasses.html
Class 2: Up to 0.99mW
Class 3R: Up to 4.99mW
Class 3B: Up to 499mW
How is it possible that the Realsense is only classified as a class 1 laser product?
-
Hi Porschefanroel The website is blocking me from posting the text of my reply, so I've provided it as an image below.
Please sign in to leave a comment.
Comments
1 comment