View my account

D455 extrinsic calibration

Comments

1 comment

  • MartyG

    Hi Jashmehta  If you are using RGB to depth extrinsics in your calculations, you may be changing the origin of the RGB image from the center-line of the RGB sensor to the center-line of the left infrared sensor (which is the origin point of depth).  This could explain why your program works correctly when using depth intrinsics.

     

    If the align processing block were being used then the origin would similarly be changed by the processing block when calculating alignment.  For example, when depth to color alignment is performed, the origin of depth changes from the left IR sensor to the RGB sensor.

     

     

     

    0
    Comment actions Permalink

Please sign in to leave a comment.