View my account

435 Error Over Time at 90fps

Comments

5 comments

  • Stevew

    Quick Note...I was concerned about heat.
    It appears the 435 shouldn't exceed 85ºC
    We are operating at about 36.9ºC

    0
    Comment actions Permalink
  • MartyG

    Hi Stevew  RealSense cameras can operate indefinitely so long as they remain within recommended temperature limits.  Officially that limit is 35 degrees C.  In real world conditions, I would expect the camera to be able to operate normally at up to 42 degrees before problems with the image may start occurring above that temperature.

     

    At 60 degrees and above, a safety mechanism in the camera firmware driver will shut off the camera's laser.  The camera can continue operating with the laser off but depth image quality will reduce and the camera may not be able to see in dark environments whilst the laser is inactive.

    0
    Comment actions Permalink
  • MartyG

    Whilst the camera can operate indefinitely whilst within temperature limits, errors and frame drops may occur if there is a non-camera problem, such as a glitch in the USB system (USB port or USB cable), or an issue with the computer hardware or its operating system.  Where such non-camera issues are occurring, it is possible for the camera to start normally and then manifest problems after hours have passed.

    0
    Comment actions Permalink
  • MartyG

     

     

    0
    Comment actions Permalink
  • MartyG

    You can use a monitoring tool such as Ubuntu's htop to monitor memory to see whether the amount available is continually falling.

    0
    Comment actions Permalink

Please sign in to leave a comment.