View my account

Comments

14 comments

  • Yu-Chern Peh

    Hi Rahul,

     

    F455 camera can be connected to Raspberry Pi 3 and 4. The Instruction for Linux is working fine for Raspberry Pi. Please note that USB 2.0 port is unable to detect the F455 camera. For Raspberry Pi 3, you need to connect F455 with USB 3.0 hub.

     

    Regards,

    Yu-Chern

    Intel Customer Support

    1
    Comment actions Permalink
  • Rahul R

    Did you see the error, this is not related the firmware which i have already update . what is the  newest version of firmware currentlly.

    1
    Comment actions Permalink
  • Rahul R

    thanks But i m having still few issue with linux setup .

     

    I m getting this error after final command run

    0
    Comment actions Permalink
  • Rahul R

    what exactly i need to pass instead of usb.

     

    0
    Comment actions Permalink
  • Karniff

    I'm also using raspberry pi. Rsid-cli program works fine.

    If you are using the latest SDK, you need to update your device firmware to the latest firmware.

     

    0
    Comment actions Permalink
  • Rahul R

    Still i'm getting same error. I tried with F450_4.0.0.37_SKU1_SIGNED.bin but it's showing below error in snapshots. 

    Replay as soon as possible. it's urgent. 

    0
    Comment actions Permalink
  • Karniff

    My raspberry pi doesn't output errors.
    I use raspberry pi 4 model B.
    0
    Comment actions Permalink
  • Karniff

    If you use the viewer program to update the firmware, please download the old SDK.

    download link : Releases · IntelRealSense/RealSenseID · GitHub

     

    There are some precautions when updating firmware.

    Update the firmware step by step.

    Ex ) If your device firmware version : 2.6.0.74 (version 0.17.1)

    Version 0.17.1 -> 0.21.0 try update ( X )

    Version 0.17.1 -> 0.18.1 -> 0.19.0 -> 0.21.0 try update ( O )

     

    I updated the firmware of the device using the above method.

     

    I don't know if it's not this problem.

    Good luck.

    0
    Comment actions Permalink
  • Rahul R

    Thanks, Problem has been solved by update firmware version as well sdk file.

    0
    Comment actions Permalink
  • Rahul R

    Do we have automatic authentication. I have connected id with raspberry pi it's working fine. but i would like to know whether it is having automatic authentication or not. if yes then let me know what exactly the process to do.

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Rahul,

     

    Glad to know you can get it to work. 

    Unfortunately, we do not have this automatic authentication. 


    Regards,
    Yu-Chern 
    Intel Customer Support

    0
    Comment actions Permalink
  • Rahul R

    hey, 

    how to update latest firmware version in linux. Do we have command to update firmware version in raspberry pi linux board.

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Rahul,

    You can update with rsid-fw-update which is generated in  \build\bin\ directory after building.

    ./rsid-fw-update --file /<download_dir>/F450_4.2.1.8201_SKU1_SIGNED.bin --port /dev/ttyACM0

     

     

    Regards,

    Yu-Chern

    Intel Customer Support

    0
    Comment actions Permalink
  • Rahul R

    Thanks ... 

    0
    Comment actions Permalink

Please sign in to leave a comment.