When the D455 is discontinued, will it stop working?
When the RealSense D455 gets discontinued pretty soon, will I be out of luck(will it completely stop working)? Or can I still use it even after it gets discontinued(as long as I buy it before)? Is there any software changes or similar that I need to do for it after it get's discontinued?
-
Hi Payaxig841 Although some camera models are being discontinued, the 400 Series stereo depth models (including the D455) are continuing.
RealSense depth cameras are not dependent on a licence / subscription or internet connection and so models that are discontinued can continue to be used without disruption.
The models being discontinued are L515 (lidar depth camera), T261 / T265 (tracking camera) and F450 / F455 (facial authentication solution)
The official Intel 'End Of Life (EOL)' public notice describing the changes to the RealSense range can be read as a PDF at the link below.
https://drive.google.com/file/d/1VWPDQPh7oRs9HNz5ngM-cUr68kUhUn_i/view?usp=sharing
Please sign in to leave a comment.
Comments
3 comments