View my account

What is the shutter speed of the realsense 435 camera?

Comments

4 comments

  • Aznie Syaarriehaah

    Hi Alexis Winters,

    The Intel RealSense Depth camera D435 is capable of capturing depth with a wide Field-of-View (FOV) of ~90x58 degrees at 90fps with a resolution of 848 x 480, producing up to 36.6 Million depth points per second. Check out these Whitepaper 'High-speed capture mode of Intel® RealSense™ Depth Camera D435' for more details. Also, you can find more information from the datasheet: https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet

     

    Regards,

    Aznie

    Intel RealSense Customer Support

     

    0
    Comment actions Permalink
  • Alexis Winters

    Hi Aznie!

    I guess I can infer an upper bound to the exposure time based on the 90 fps maximum. I'd really like to see a specific shutter speed spec in the datasheet though (which I cannot currently find, and this is different measurement than fps, even though fps does depend on shutter speed).

    0
    Comment actions Permalink
  • Aznie Syaarriehaah

    Hi Alexis Winters,

    Shutter speed/exposure time is an adjustable value in the RealSense Viewer under control. You can view the value from the RealSense Viewer.

     

    Regards,

    Aznie

    Intel RealSense Customer Suppor

    0
    Comment actions Permalink
  • Alexis Winters

    What is the minimum exposure time I can set?

    0
    Comment actions Permalink

Please sign in to leave a comment.