View my account

Is there a product like the T265 (pose data important) that I can generate a trajectory with?

Comments

3 comments

  • MartyG

    Hi Chutchinson  The D435i stereo depth camera model does not have built-in support for pose stream data like the T265 Tracking Camera model does.  

    If you want to obtain pose (position + angle) of the camera itself and not an observed object then whilst it is straightforward to retrieve roll, pitch and yaw from the camera's internal IMU component, the main challenge is obtaining the XYZ position of the camera relative to its current location in a scene.

    You may therefore be interested in an adaptation of Intel's D435i SLAM navigation guide for ROS. The adaptation adds localization and the ability to track and display the camera's relative position compared to a loaded map.

    https://shinkansan.github.io/2019-UGRP-DPoom/SLAM

     

    The original Intel guide that does not include camera position information is here:

    https://github.com/IntelRealSense/realsense-ros/wiki/SLAM-with-D435i

    0
    Comment actions Permalink
  • Chutchinson

    I do not have a map to load.  I need to use it more like the T265. I did look at the Navigation2 tutorial but it looks like I need an existing map.

    https://intel.github.io/robot_devkit_doc/pages/navigation.html

     

    0
    Comment actions Permalink
  • MartyG

    In SLAM navigation, a map of a location can be recorded by having a robot patrol the area that it will be used in and progressively build up the map as it travels.  When it is decided that the map is sufficiently detailed, live recording is stopped and that pre-recorded map can then be used by the robot during live navigation to avoid obstacles.  This is referred to in the Save Map Data section of the DPoom guide linked to earlier.

    0
    Comment actions Permalink

Please sign in to leave a comment.