View my account

L515 ToF working principle

Comments

3 comments

  • Zulkifli Halim

    Hello Evacurto,

     

    Thank you for contacting us.

     

    The L515 Camera uses LiDAR technology to measure the distance from the camera to the object. Similar to other LiDAR systems, the L515 sends a laser beam and measures the returned time of the reflected light off an object. The L515 accomplishes this using a continuous coded IR beam. The time taken for the light to return to the camera is used to calculate the distance of the object.

    For more detail please visit Optimizing the Intel RealSense LiDAR Camera L515 Range.

     

    Sincerely,

    Zulkifli Halim

    Intel Customer Support

    0
    Comment actions Permalink
  • Evacurto

    Hi Zulkifli, 
    Thanks for the reply. 
    I know that L515 is a Lidar and that uses the difference between the emitted and returned light to measure distance. What I really want to know is how the laser beam is codded and the expression used to estimate depth. I know that ToF distance measurement can be based on single-pulse modulation or harmonic modulation (measurement of phase delay Φ). Since the IR beam is continuous I must assume that the measurement is based on continuous harmonic modulation? In that case, can I assume that distance is estimated by D = (c. τ)/2, where c is the speed of light and τ is Φ/(2.π.f)?  
    Thanks!

    0
    Comment actions Permalink
  • Zulkifli Halim

    Hello Evacurto,

     

    Yes, the formula for depth is D = c.ΔΦ/(4.π.f). You can refer to the Introduction to Intel RealSense LiDAR Camera L515 video (minutes 11 to 15) for the explanation of the L515 working principle.

     

    Sincerely,

    Zulkifli

    0
    Comment actions Permalink

Please sign in to leave a comment.