Do D435 driver and firmware support Windows 10 21H2?
Hello,
A customer of mine asks if D435 driver and firmware already support Windows 10 21H2. If not, will you please tell me when they will support Win10 21H2.
Regards,
Ohara
-
Hi Shigeyoshi Ohara Yes, RealSense 400 Series cameras such as the D435 model cameras are compatible with Windows 10 21H2. I have 21H2 (also known as build 19044) on my main RealSense work computer, shown in the image below. It is also on my personal PC that I successfully use RealSense cameras with.
-
It should not matter which SDK or firmware driver version is used with the camera on Windows 10. If your customer wants a configuration that they can feel assured about though then they could use Intel's recommended production camera configuration (one that can be used reliably with critical applications and commercial products that incorporate RealSense).
Intel's current recommended Production configuration at the time of writing this is SDK 2.50.0 and firmware driver 5.13.0.50
https://dev.intelrealsense.com/docs/recommended-production-camera-configurations
Please sign in to leave a comment.
Comments
4 comments