View my account

more noise at 1 m distance than 0.5 m

Comments

1 comment

  • Zulkifli Halim

    Hello Rachel,
    Thank you for contacting us.
     
    This might be due to the short range preset. This preset lower the laser power and gain so that close objects do not oversaturate the receiver. This allows operation at a close distance to objects. This setting may not be good if objects further away in the scene also need to perform well. 
     
    Note that the depth-sensing of the L515 works best in low-light conditions, the less light the better.
     
    You may refer to L515 User Guide for more information.
     
    Sincerely,
    Zulkifli Halim
    Intel Customer Support 

    0
    Comment actions Permalink

Please sign in to leave a comment.