Multi Sensor Synchronization
Hi. I'm using two L515 sensors and want to connect them as synchronous.
I've found the resource(https://dev.intelrealsense.com/docs/lidar-camera-l515-multi-camera-setup) which succeeded to connect sensors as synchronously. However, It's hard for me to connect as cable, and I want to synchronize through the Realsense SDK 2.0. Therefore, I'm trying to use the USB 3.0 hub(iptime UH305) for synchronizing two sensors. I've enabled the Inter_Cam_Sync_Mode in Realsense SDK 2.0, but I can't reach the next setup and need your help.
Many thanks.
-
Hello Joo,
Thank you for contacting us.
What computer are you using (PC, Nvidia Jetson, Raspberry Pi, etc) and which OS did you use?
As described in Section 2 Parts A to D of the L515 multiple camera paper, a range of factors can affect the performance of the multiple camera setup, including the number of cameras used, whether the cameras are attached to a USB hub, and the capabilities of the computer hardware.
Sincerely,
Zulkifli Halim
Intel Customer Support
Please sign in to leave a comment.
Comments
1 comment