Roman Leuzinger

  • Total activity 26
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 7

Activity overview

Latest activity by Roman Leuzinger
  • Roman Leuzinger commented,

    Thank you for the response. However, I'm referring to the cutout that is located on top of the dot projector (the IR filter has a hole where the dot projector is located). Technically, the IR light...

  • Roman Leuzinger commented,

    I understand that but there are other warnings that I don't want to suppress.

  • Roman Leuzinger created a post,

    Resource temporarily unavailable, number : 11

    We are testing the realsense on our robot and we are using ROS. At certain points, we change the exposure of the stereo camera periodically. Whenever we do that, the following error message is spam...

  • Roman Leuzinger created a post,

    IR Filter Cutout

    Hello there, We are exploring the use of RealSense cameras in our product. We are looking into buying D435 modules but need an IR-Filter to be mounted. The D435f has a cutout for the dot projector,...

  • Roman Leuzinger commented,

    Not other than recommended in the datasheet. We have a source but many options to choose from.

  • Roman Leuzinger commented,

    What kind of adhesive layer is used to stick the lens cover into the housing? Is this IP54? Why is the NIR filter in front of the lens cover? Will there be problems if the NIR filter is mounted beh...

  • Roman Leuzinger commented,

    We have opened a D435 to learn more about the integration and it really helped to see its parts. I am already in contact with Cocom for the flex interposer. I will get all the details from there. E...

  • Roman Leuzinger commented,

    Is the interposer 82635DSITR50P the original part from the D405? What part is used in the D435?According datasheet the interposer of D435 is not straight and is different from the listed part. That...

  • Roman Leuzinger created a post,

    D430 integration (function of optical elements)

    We want to install the Depth Module D430 and the Vision Processor D4 in a customised housing.Do the left / right imager and the IR projector always have to be isolated with a gasket? Even if a two-...

  • Roman Leuzinger commented,

    Could you give me some more information about the mentioned interposer which can be a rigid circuit board that can be purchased pre-made?- Manufacturer- Produt name and numberIt would be interesset...