Javier
- Total activity 13
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 4
- Subscriptions 5
Activity overview
Latest activity by Javier-
Javier commented,
Wan, thank you for sharing this information. Just to confirm, can the D457 USB port perform and operate like the D455? (Assuming we follow your instructions). Some of us need the IP65 grade enclosu...
-
Javier commented,
What is the reason that the D457 camera cant be used as a USB "plug and play" camera like the D455? Can someone (that is actually using the camera) confirm if the USB port can be used for developme...
-
Javier commented,
was planning to use the D457 model for a volumetric measurement use-case in the construction industry. Any cost-effective way to work with the GMSL FAKRA interface?
-
Javier commented,
Can we at least use the USB port for development purposes?