Oriol Vila
- Total activity 4
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Oriol Vila-
Oriol Vila commented,
I see, seems that the CustomRW tool is the only way to do so. It would be helpful that in future versions of the SDK, the Y16 parameters could be retrieved as they are stored somewhere in the devic...
-
Oriol Vila commented,
As you said, the coefficients are set to zero for the stereo matching. Therefore when I get the intrinsic parameters of the rectified infrared stream they are all zero. The problem is that I want t...
-
Oriol Vila created a post,
Intel RealSense D415 get intrinsic parameters using the API (pyrealsense2)
I’m developing my custom calibration application using python and pyrealsense2 and I would like to initialize the intrinsic parameters using the factory calibration of the device. But I have not fo...