Lyhour Newtechnology
- Total activity 28
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 1
- Subscriptions 7
Posts
Recent activity by Lyhour Newtechnology-
How to save point cloud with RGB information using Python?
My camera is L515. I used to generate the point cloud from the Intel Realscense viewer. It works fine which I can get the point cloud *.ply file. Also, in the *.ply file contains the location X,Y,Z...
-
receiver light saturation, stream stopped for 1 sec for L515
During I am streaming the depth sensor, it always occur the problem of receiver light saturation, stream stopped for 1 sec. It induces the the flash during the streaming really annoy. I record vide...
-
what is depth value generate from L515 ?
when I save the depth frame data, I notice about the value (pixel) of the depth. I want to know what this value represent for ? does it represent the distance between the Camera to the correspondin...
-
How to configure L515 Min distance controls in python ?
Hello everyone, I am writing the python code to capture the RGB, depth and IR for creating the dataset by using the L515 device. I want to configure the property "min distance" as in the intel real...
-
How to align infrared resolution the same as RGB resolution ?
Hello Everyone, I use these codes to align the depth and IR to the RGB resolution. However, I can achieved only the depth data that is the same with RGB. I want to know how to configure or align th...
-
How to get depth information (depth pixel) and extract the *.raw file ?
Hello everyone, I am using the L515 for capture the RGB, Depth and IR of the pavement surface. Currently, I am working on RGB-D object detection. I am acquiring a new dataset for my detection. Ther...
-
Is it possible the L515 capture the depth of aggregate (rock) ?
I recently bought the Intel Realscense Lidar L515. I want to know how to capture the depth of the aggregate (rock) as shown in the image. After I get the depth information of the aggregate, I want ...