Guopengzhen2015
- Total activity 15
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 7
Activity overview
Latest activity by Guopengzhen2015-
Guopengzhen2015 created a post,
Severity: 1, Code: 16, single frame error
when I use the sdk , I got an error as following: what does this mean?
-
Guopengzhen2015 created a post,
RealSenseActivationTool problem
I got two product key, but I use them in one camera , how can I resolve one. And use it on another camera.
-
Guopengzhen2015 created a post,
-
Guopengzhen2015 created a post,
Intel Realsense DIM Weight Software and RealSenseActivationTool problem
I have two L515: then I need to use DWS, so I make license with same product key and email, but one serial number is ok, another failed; the success one license, I use at DWS viewer,but :
-
Guopengzhen2015 created a post,
L515 DWS SDK why cannot find multi boxes
In the example code , this is a callback func has box_count , but when I test with two boxes( can be find one by one), they cannot find both; static void * _dim_callback(int frameId, int box_cou...
-
Guopengzhen2015 commented,
Thank you, I got it.
-
Guopengzhen2015 commented,
yes, it's in the same directory.After that, I found new errors. If I run the '.exe' directly (not run in Visual studio 2019),I got some error as follows:
-
Guopengzhen2015 created a post,
L515 DWS SDK static_mode_config.json parsing failed
IDE: visual studio 2019 code is example code in <Intel® RealSenseTM Dimensional Weight Software (DWS)> I have add lib by fallowing instruction;