A M Handley
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by A M Handley-
A M Handley commented,
Hi Wan, This article is for the D415 or the D435. Are the same tuning settings for the L515? Adam
-
A M Handley commented,
Hi Wan, We are using the camera at 1280 x 720 at a distance of 0.5 - 1 m from the wall. We are using the SDK at version 2.50.00, the latest version that the L515 was supported with. The firmware ...
-
A M Handley created a post,
Low Frequency Oscillations in Depth
Hi, I have taken a recording of a blank wall to test the depth consistency of the L515 camera. The recording was collected using the capture function of the MATLAB wrapper that has been adapted to...
-
A M Handley commented,
I also have this issue. Thanks, Adam