Jesus. Garcia
- Total activity 132
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 7
- Subscriptions 64
Activity overview
Latest activity by Jesus. Garcia-
Jesus. Garcia commented,
Yes, a longer baseline would allow depth sensing much further but trade-offs have to be made based on target usages. The T265 is the only camera that provides pose information. The D435i, D455, and...
-
Jesus. Garcia commented,
Hello Chicagobob123, What enables the D455 to detect depth further than the D435 is the longer baseline of the D455, which is the distance between the two depth senors. D435 Baseline: 50mm D455 Bas...
-
Jesus. Garcia commented,
Official comment Hello Chicagobob123, The facial data is stored as an encrypted binary blob on a Secure Element in the F400 module. The Enrollment Process explains it a bit further. You should also read the dat...
-
Jesus. Garcia commented,
Hi Zack, The RealSense LiDAR Camera L515 will not work well outdoors. It works best indoors with as little ambient light as possible. Intel does not sell components that will allow you to build you...
-
Jesus. Garcia commented,
Hello Tledger, Please provide more information to help us troubleshoot: Does the pre-built RealSense DWS Viewer work? What platform are you running on? Make/model of PC, processor, amount of memor...
-
Jesus. Garcia commented,
Hello Anoop, Did you copy the full contents of the RealSenseDWS_SDK folder into your project's $(TargetDir), where your executable resides? In your sample.cpp file, include "DEBUG_DWS_Sdk.h" Sincer...
-
Jesus. Garcia commented,
Hello Arpit, Below are instructions for enabling debug mode and gathering logs. However, logs may not be created in your case because the program does not get that far due to the low processing pow...
-
Jesus. Garcia commented,
Hello Arpit, It is possible that the DWS software cannot run on your NUC because of lack of processing power. Your NUC has a Celeron processor that was released in Q4'17 and only 4 GB of memory. O...
-
Jesus. Garcia commented,
Hello Arpit, Do you still need help with this issue? Sincerely, Jesus G. Intel Customer Support
-
Jesus. Garcia commented,
Hello Anadig, I misunderstood your question. You are using the binary installation of the RealSense SDK which does come with OpenCV. If you build the RealSense SDK from source you can use whichever...