Jerry
- Total activity 25
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 6
Activity overview
Latest activity by Jerry-
Jerry commented,
hi marty - with my case (detecting depth changes on a table top 2m away from the camera) which is the best setting ? Do you think the changing the A-factor will have a beneficial effect on the RMS...
-
Jerry created a post,
How to get actual Infra Red image with 415
Hi ! Has anyone managed to get an actual IR image without any of the visible light ? The example in the SDK (Unity wrapper) is a mix of both I think as I can read the print on books that I hold in ...
-
Jerry commented,
Hi Marty (and anyone else) - just two questions here. (1) I'm unable to reduce the noise created with the depth image once the objects are +1.5m away from the camera - no lighting setup or surface ...
-
Jerry commented,
btw. it's freezing because OpenCV cant handle the image it's receiving from the camera.
-
Jerry commented,
hi Marty - when I remove the max distance from the depth cutoff feature it just freezes Unity. This is the same as when i set the max distance to be beyond the wall. Also - wouldn't it just give m...
-
Jerry commented,
sorry Marty - i didn't explain that properly - the camera & projector are directly in front of the screen (i took the photo from an angle without thinking) I'm trying to pick up objects as close to...
-
Jerry created a post,
415 depth sense granularity
I'm projecting onto a surface and using the 415s point cloud to sense objects on it (because point cloud allows depth cutoff and the 2d doesn't - in the unity wrapper anyway) Here's my setup - 3 vi...
-
Jerry commented,
hi marty - I'm now using the point cloud data because it can do the depth-cutoff that the 2d depth scan can't. I'm passing the resulting image into openCV to get it blob-detected and the problem f...
-
Jerry commented,
yup - it's the projector. When I turn it off the noise stops. I'll try see if i can dim it a bit - although that will impact the image quality somewhat. two steps forward eh?
-
Jerry commented,
hi Marty - based on your last post I've switched from 2d to 3d to use that depth cutoff - and am running the result into a texture that gets blob detected. The cut-off part works which is good, bu...