Nikhil Kasturi

  • Total activity 7
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 1
  • Subscriptions 2

Activity overview

Latest activity by Nikhil Kasturi
  • Nikhil Kasturi commented,

    Dear Phillip, Was referred to you by a colleague of yours, Mr. MartyG. I have two questions for you (unrelated to wheel odometry): 1. What is the smallest increment of change in pose (meters) that ...

  • Nikhil Kasturi commented,

    Will do. Please note that my questions have nothing to do with wheel odometry. Cheers,Nikhil

  • Nikhil Kasturi commented,

    Dear MartyG, Perhaps I should rephrase my questions. 1. What is the smallest increment of change in pose (meters) that the T265 can detect and output? 2. Assuming the orientation of the T265 is qua...

  • Nikhil Kasturi created a post,

    Intel T265 SoftCalibration and Resolution.

    Hello, 2 Questions: - What is the max resolution for pose data (1mm, .1mm, ...)? Nowhere is this stated in the tech specs.Note: Sample app gives precision to the closest millimeter (SDK 2.0).- I kn...