Mau
- Total activity 25
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 8
Posts
Votes on activity by Mau-
D455 suddenly not detected, completely gone!
We have a RS D455 camera connected to an AGX Xavier, it was working fine for a long time, however, it has disappeared and is not reachable. There are also other cameras connected to the AGX Xavier...
-
D455 Poor Depth Performance
Since a while back, we are having issues with the accuracy of the depth measurements on the D455. It used to be really good, however, now I cant manage to make it work like it used to. This is like...
-
My L515 built-in filter is broken
Hello, While opening the camera, I cracked the front glass on one of my L515 cameras. It seems like without this filter the camera still works but I cant get it to see well (not as accurate as I r...
-
D455 Screen Tearing/Flickering Issue
Hi, We are using a D455 for a video analytics project, its a great camera, however we are experiencing an unusual issue where sometimes the video feed gets corrupted and the screen seems to be stu...
-
Can I assemble a better than the D455?
Hello, We have been successfully using the D455 camera for long range (7 meters) applications and it performs really well. Nonetheless, I have been thinking for a while if it would be possible to...
-
D455 Max Depth Range 20m or 5m?
Hello, I have been testing the D455 for max range hoping I will be able to measure objects 7meters away. However, I have not been able to do that as the depth camera seems to only see until 4-5 met...
-
Buying the D430 and D415 Depth Modules and Vision Processor
I am developing smart cameras that use deep learning and computer vision to detect events. I am developing the software and assembling the hardware, thus, the RealSense vision processor and depth c...
-
Low-light conditions or night vision with D415
I just started with the D415 and I have been able to use the RGB and depth cameras, however, I need a camera that can also see at night. From the tests I've done the camera does not see well during...