Jimmek
- Total activity 19
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 2
- Subscriptions 5
Activity overview
Latest activity by Jimmek-
Jimmek commented,
We have made some progress and have not heard back from you. We would very much appreciate your help in confirming the following regarding the D455 cameras. Note that we have confirmed that the cam...
-
Jimmek commented,
Hello MartG and Garcia, Referenced Whitepapers: 1. Using the Intel® RealSenseTM Depth cameras D4xx in Multi-Camera Configurations 2. External Synchronization of Intel® RealSense™ Depth cameras Firs...
-
Jimmek commented,
Marty G, Where can a developer for syncing two D455 cameras in 1) master/slave mode (fixed FPS), and 2) both cameras in Mode 4 where there is an external pules train / trigger (variable FPS) as inp...
-
Jimmek commented,
SW SDK Win10 ver 2.4.1.0.2657 FW ver 5.12.10 Cameras two D455 Still having a problem having one camera as Master (1) and another as a Full Slave (3) using Viewer. Cable connection pin 5 to 5 (si...
-
Jimmek commented,
Progress Update and Trouble-Shooting Questions. For an external trigger for HW sync, an alternative to an Arduino Micro referenced in "External Synchronization of Intel® RealSense™ Depth cameras"...
-
Jimmek commented,
Thank you Marty for the reply. I reviewed the referenced material and have a few more questions. After everything is setup using viewer for one master(1) and one slave(3) where a sync cable connect...
-
Jimmek created a post,
Syncing two D455 Cameras, one as master and one as slave unsuccessful
Cameras: two D455s S/N 037322251516 S/N 037322251668 FW: 5.12.09.00 SDK and Viewer 2.40.0 Win 10 PC New with Intel 7 CPU Been unable to get cameras to operate in sync master/slave mode. I ha...
-
Jimmek created a post,
Specs Regarding 1.8V External Sync
Documentation for using external sync for D455 cameras has the trigger voltage level as 1.8 V . What is the tolerance level for this 1.8V signal? Is the non-trigger state 0 volts and is there a t...
-
Jimmek created a post,
D455 configuration, saving, recording
From the RealSense viewer UI, various RGB, Stereo, Depth, and Tracking settings can be set by the user. Can all of these settings be saved to a file or files for later recall/loading/importing? Is...
-
Jimmek commented,
Thank you MartyG. I will look review these links.