Stevew
- Total activity 41
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 2
- Subscriptions 13
Posts
Recent activity by Stevew-
435 Error Over Time at 90fps
With a diagnostic tool running, I've allowed the 435 cameras to run overnight.At the 4hr mark, the errors were nominal.Over time, were seeing the Critical Frame Drops start to add up dramatically.(...
-
Should we update Firmware?
General question.We've been using the 435 for several years now,.We locked into FW v5.13.00.50 during development.(newer FW versions require adoption of a new SDK)Looking at newer updates in firmw...
-
435 USB 3.0 and Static
Noticing, especially this time of year, a lot of static related issues.We use these cameras exclusively with Windows PCs.In high static environments, the Cameras disconnect from the PCs.They won't ...
-
435 Calibration Stability
When we receive a shipment of cameras, we test their calibration to make sure they are within our operating spec.If necessary, we do a quick calibration on them...I've seen some returns lately, and...
-
Adding Additional IR to the Scene, can it be helpful?
Our team has been sending out supplementary IR light since our product release.(It's never been explained well, and I've always considered it witchcraft. I've no evidence it's ever helped.) Today ...
-
FOV vs. Output Resolution
I'm trying to rectify something in my mind, I'm sure is simple.I'm not a programmer, I don't have experience with the SDKLooking at the 455 (depth) Field of View: 3:2 Output Resolution: 16:9 How...
-
New Error with New 435 Delivery: Auto Gain Limit
Our assembly team just received a new batch of Intel 435sUnlike (all) previous deliveries, they error immediately in the Realsense Software.The error (also seen in attached image):Invalid Value in ...
-
Trying to understand results of 455 Test
I can't add video here, so I've added a pic of a quick 455 test.This is just down a hallway outside my office.You will see the depth measurement is roughly 13' (which is roughly where the device is...
-
RealSense Website Errors: Reference #102.a22d2d17.1663621817.14465e44
Getting a number of Intel RealSense Website Errors as I try to find information to help with an some problems we're having with the 435Getting them in links on webpages and in documentation.Thought...
-
Calibration Error (response -7)
Having difficulty calibrating the 435 inside the RealSense ViewerGetting: Calibration Failed Invalid Value in rs2_run_on_chip_calibration_cpphwmon command 0x80(8 3 0 /) railed (response -7) Tried...