Mohammadmahmoodi8020
- Total activity 21
- Last activity
- Member since
- Following 1 user
- Followed by 0 users
- Votes 0
- Subscriptions 5
Comments
Votes on activity by Mohammadmahmoodi8020-
I appreciate it.
-
I removed 5.12 with Revo Uninstaller to be sure there is no registry or leftover folder. In 5.11 I got another error code. The error 9998 (unknown)
-
I downgraded to 5.13.0.50. I was using the original 1m cable. nothing changed.
-
I remember two of my cameras had 5.13.0.5 and they had the same issue.
-
I already installed 2.53.1. Is there any problem with downgrading?
-
Unfortunately, the same results.
-
yes, I did. I'm using USB 3.0 and also a high-quality USB 3.0 cable. besides, I checked the Realsense viewer for checking my connection is USB 3.2.
-
I installed the RealSense UWP driver. The results are the same. The on-chip calibration is working for me but the results are not satisfactory. I always get better results with the Dynamic Calibrat...
-
I'm using D435 and Windows PC with a direct USB 3.0 connection. Both the Realsense viewer and Calibration tool apps are updated to the latest version.
-
Thank you for your kind reply, I already did it and also reinstall the 5.14 firmware. Unfortunately, the problem still persists.